Other Parts Discussed in Thread: OPT3101, FDC1004
Hi TI team,
Do you recommend using FDC2212 for wave-hand detection or proximity sensing?
Any limitations of using FDC2212 for such kinds of applications?
Thanks.
Hector
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Hector,
The FDC2212 has issues with stray capacitance causing false triggers. As such you would need to devote alot of effort to designing your system such that the stray capacitance is eliminated or reduced. FDC1004 addresses the stray capacitance issue with active shield driver, yet we typically only recommend that for water level sensing. A better alternative to consider might be the OPT3101.
Hi Patrick,
Thanks for pointing out this.
Do we need to put a lot of effort into designing the shield to reduce stray capacitance?
Hector
Hello Hector,
According to my colleague, it can be quite challenging if you have not designed one before. Apparently, out of the known attempts, only a very small percentage have actually taken their product to market with the FDC2212 solution. I personally have not designed with FDC2212 and a lot of our team is out due to the holidays. When one of our applications support who is more experienced with this device returns from the holidays, I can ask if he might have some tips to share. In the mean time, this link and this link might give you some ideas for reducing the stray capacitance. Another thing worth mentioning is that your system ground will also affect detection distance. If ground is relative to a battery as opposed to earth ground, your possible detection distance will be shorter.