Part Number: TMCS1101
Other Parts Discussed in Thread: TMCS1100,
Hi Team,
My customer is asking if TI have current sensor that fits following requirement, could you kindly help?
Voltage rating : around 500V dc
Resolution : better than 50uA
Regarding voltage rating, TMCS1100 and TMCS1101 supports 600V working voltage so 500Vdc should be okay for TMCS1100 and TMCS1101, right?
And from this thread, I think resolution depends on the bit of ADC and Ax variant of TMCS1100 and TMCS1101 customer uses.
If customer uses 20 bit ADC with 5V and A4 variant(400mV/A sensitivity) of TMCS1100 and TMCS1101, customer can fulfill 50uA resolution, is it correct?
If so, I will recommend TMCS1100 and TMCS1101 to customer.
Thanks.
Regards,
Jo