This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2080: Question Asking

Part Number: HDC2080

Hi Team,

My customer want to use this sensor ic, do they need to add MCU to turn to USB interface?

If yes, do we have reference design or which MCU is suitable for this sensor ic?

  • Hello,

    The HDC2080 is a digital temperature and humidity sensor which uses I2C bus for communication. A microcontroller or processor is required to control and communicate with this device. We have used a variety of MCUs such as arduinos, MSP430s and other MCUs to calculate the measurements. The choice of MCU will depend on you end application (based on power settings, features, etc.).

    This link includes an informative video, and has library files for the arduino IDE.

    Regards,
    Pavani Tenneti