Dear Team,
I was wondering if at this moment there is some software examples / drivers / library available for the TMAG5273?
I read in a different thread (from 5 months ago) that there wasn't at that time. But for this time it seems to me that there needs to be, because;
I have the evaluation module of the TMAG5273, For this evaluation module I can download some firmware on your website on the following URL: TMAG5273 data sheet, product information and support | TI.com
This download only comes with the firmware-image and this works fine on the evaluation module. But now I want to implement this kind of software myself on a custom PCB. On this PCB I already implemented the I2C drives/software myself but it would be very handy (and speed up the development process) if there would be any posibility to get the source files. (or only the specific source files in which the protocol/communication to the sensor is implemented)
Sincerely,
Tim von Unen