I want to detect vehicles using AOP device, which is the best lab example I can consider as the base of the project?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to detect vehicles using AOP device, which is the best lab example I can consider as the base of the project?
Hello,
A few things to note. Our demos specifically for detecting cars are optimized for longer distance, so they don't support the AOP device as, and will require code changes. They both are made to use the ISK antenna / EVM. What kind of distance are you needing to detect cars at? The AOP device will be somewhat limited in max distance due to the antenna pattern.
If you are trying to detect parked vehicles, then the Parking Garage Sensor lab is the best to start with.
If you are trying to detect moving cars, then the Traffic Monitoring Demo is the best to start.
Both of those use the IWR6843ISK. It seems in the previous question you want to detect parked cars with the AOP. In that case, you can use the Area Scanner Demo. This is very similar to the parking garage sensor demo, but it supports the AOP antenna configuration.
Regards,
Jackson
Hello, if you just want to detect cars within a short distance, and use the AOP device, using the area scanner lab is probably best. You can ignore the static objects if you chose. It will be tuned for a shorter distance. You can see the CFG parameters from the parking garage sensor lab (which has the same embedded SW mostly) to see how to modify the chirp parameters for cars. Switching to the AOP antenna is difficult as it requires a new angle estimation procedure that is not included in the traffic monitoring demo.
Regards,
Jackson
This depends on how you want to 'detect' cars. If you want to track them as they are moving, you will want to modify the gating parameters of the tracking configuration. Please see the following document. 3D_people_counting_tracker_layer_tuning_guide.pdf
If you are using the static object detection, you will want to modify the parameters for the static config. Please see the following document.
https://dev.ti.com/tirex/explore/node?a=VLyFKFf__4.10.1&node=ANeAbdL5iuCGKCHkfAqZgw__VLyFKFf__4.10.1&r=VLyFKFf__4.1.0
Regards,
Jackson
Yes this should be all that is needed. Just make sure to adjust the boundary box commands as well to set the tracking boundary.
Regards,
Jackson
I'm trying to change the cfg file by checking the traffic monitoring 3d file into the area scanner aop file.
In tracking commands, for stateParam and trackingCfg, the parameters defined or not the same. Either one parameter is more or less in one of them and I'm getting errors while i run the gui of the area scanner.
Also I'm referring to the 3D_people_counting_tracker_layer_tuning_guide.pdf document for configuring and understanding the parameters.
Could you help me if the number of parameters are constrained in AOP deivce?
Hello,
The difference is not in the AOP device, but in the SW in those demos. They use different versions of the tracker and the command structure is a little different. The documentation should apply well to the traffic monitoring demo, but less so to the Area Scanner demo. To understand the exact parameters needed, it will be best to go look in the code to see which params are needed. The file to check is mmw_cli.c at the following path.
C:\ti\mmwave_industrial_toolbox_4_10_1\labs\Area_Scanner\src\68xx\mss
There is also a similar file in the traffic monitoring demo.
Regards,
Jackson
I have attached the screenshot of mmw_cli.c file which i referred to, it looks same but I'm not sure how are the parameters are more inside the cfg files.
The cfg files also i have attached which I'm referring to where i see the parameters are not same.
Could you please tell me how to resolve this and also if I'm referring to correct files?
Hello,
I think the help strings are not accurate in all these demos.If you go to the command handler function for those CLI commands (e.g. MmwDemo_CLITrackingCfg), it will show you the difference in how each of those are being used. The variable assignments will look something like the below image.
Those functions will be in the tracker_utils.c source file, which is linked to at the top of the mmw_cli.c file.
Regards,
Jackson
Thank you, i figured out for the Stateparam how to fix but not for trackingcfg.
I can directly change the files of area_scanner_68xx_mss lab project code for AOP right?
When i build the system, it's showing for ISK, I'm bit confused here, if we have project files for AOP or not?
The Area scanner demo has different build configurations for the different antenna configurations. You will need to select AOP from the build hammer drop down in CCS.
Regards,
Jackson
If you have changed the format of the CFG file, you will need to change the format of the CFG parser in the GUI files. If you just changed the values, there should be no issue. The demos may not be compatible with other GUIs however, so if you change which GUI you are using, you will need to check the CFG parser to ensure compatibility.
Were there any errors in the GUI console? you may need to run the .exe from the CMD console so that the errors stay if you close the program. Or if you run from matlab source the errors will show there.
I think maybe we should levelset, as there have been many changes. Can you post your CFG file and which BIN and GUI you are trying to use? It seems that you are using the area scanner BIN file and GUI but the traffic monitoring CFG? Is that still true?
Sorry, it did not resolve my issue by mistake it happened.
Yes, you are right. I have attached both the files. I have changed the values and have commented few of the traffic monitoring parameters inside the area scanner since it is not working in the GUI when i execute. It says something like it cannot read the values (I don't remember exactly the error, once I reproduce it, i will post it).
Please let me know which other files I need to consider?
Thanks Harish,
I will look at this later today and get back to you with some suggestions early next week.
Regards,
Jackson
Hello,
It looks like the .bin file you sent does not boot fully. Are you using the default AOP bin for area scanner, or have you modified the source code?
Also, that error means that the sensor crashed after sending the CFG. This is very unlikely to be caused by the values in stateParam, more likely there was a code change that causes this.
I don't see anything in the CFG file you sent that shouldn't work with the area scanner demo, however the values in gatingParam and maxAccelration are very large and will probably cause detection issues. Also, you have modified your boundary box to be very large. There is no problem with this, just note that the AOP device will not get any detections at the far values you have.
Regards,
Jackson
I have again attached the .bin file which has some code modifications in it adding the extra parameter whcih is needed for the StateParam as the initial step I have done. The build is successful and also i can dump the code into the hardware using this file.
The values in the cfg file, I have taken it from Traffic monitoring as an initial step to just get started, later fine tuning the values is the thought process. Since, I'm unable to execute it successfully, I'm stuck at this point. Even the COM ports, don't detect properly and they are sporadic sometimes. Could you help me how to proceed further?
6471.area_scanner_68xx_demo_aop.txt
For hardware issues: I have a thread here:https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1088208/iwr6843aop-iwr6843aop
Hi Harish,
Please make sure you are following all the steps in the user's guide correctly when rebuilding the project, as this binary does not start up. It seems the changes you have made stop the program from booting correctly. Did you change anything besides the CLI file? Did you build the DSS image before building the MSS image? Did you select AOP for both builds?
Regards,
Jackson
Also, if you are just trying to use longer range detection with the AOP and area scanner, please try the following CFG file with the default area_scanner binary file for AOP.
area_scanner_68xx_AOP_longRange.cfg
The antenna pattern of the AOP device may not work well for detection longer than 20m or so, maybe less depending on the object.
Regards,
Jackson
I have also changed tracker_utils.c since the parameters had to be changed for StateParam. I changed the configuration in properties and made the AOP device active: I had compiled only MSS and did not touch DSS folder at all. Is this the issue?
Should I compile first DSS and later MSS?
Yes, you need to build the DSS project first and then build the MSS project. If you only build the MSS then there is only half the device code in the binary. The MSS project has postbuild steps to combine the DSS and MSS .out files into a common image. These instructions should be in the user's guide.
The area you want to detect cars should be set with the boundaryBox cfg. Currently it seems very large in your configuration so should not limit your detection.
Regards,
Jackson