This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1101: LDC1101

Part Number: LDC1101

 VDD is powered from 3.3V digital and ground and the Rp values are excessively noisy. Don't have the common mode filter laid out on the board, so I only have the two 0402 EMI caps on the INA/INB pins to ground to mitigate EMI susceptibility. Would the noise be less if I run the sensor IC from a 1.8V LDO like on the EVM board?