Hello everyone,
How is the sample rate of OPT3101 calculated for Super-HDR mode?
In Non-HDR mode the formula is:
In Auto-HDR mode one additional sub-frame is added: with HDRmode = 1.
Is it the same for Super-HDR mode or is here a second additional sub-frame added for validation of the amplitude?
In my application OPT3101 is used in Super-HDR mode with an averaging filter of 16.
So for Non-HDR mode sample rate would be 4000 / 16 = 250 Hz.
For Auto-HDR mode sample rate should be 4000 / 17 = 235 Hz.
Against theory, I measure for my application in Super-HDR mode a sample rate of about 248 Hz.
Measured with Data_Rdy signal on GP1 pin.
Configuration was done with Configurator Tool and SDK.
Is there an explanation for this sample rate?
Thank you.
Stefan