I'm using CCS studio for making my changes in the code of one the lab examples.
Since the lab example codes are placed in ti folder which is used for build for the lab examples. I have imported them from the CSS project from one the lab examples and made my changes in the code. Inorder to have the whole project at one place how can i export the project?
When i export at area_scanner_68xx_mss, the mss folder which has files in ti folder are not exported and the whole project is not at one place which is difficult for me to handle the project separately. Could you help me how to have all the project files at one place and build in CSS?