- Part Number: AWR1843BOOST
Hi TI Team,
Good Day!
Can you please let me know the solution for the following issues:
1)if there is any specific configuration, that you can recommend to get the obstacle detection for atleast 50 meters (for objects like Car / Truck).
As of now, Even large objects are detected at only 20 meters and not at a greater distance(at least between 30 to 50 Meters)
I have tried to use some of the config files shared to me by TI team, without Z Values (Elevation), while using those config file, I get obstacles detected at over 40.meters, but if the config is added with Z value(Elevation), the distance of the obstacle detection is reduced.
2) While driving the Car on highways with RADAR fixed(as shown in the pic)
I suddenly get a burst of false positives on an empty road with no obstacles for next 200 meters, Can you please help me, to reduce the same with the help of Configuration Values.
Also, Can you please let me know, why sudden burst of false positives encountered on an empty road, even if the elevation value is controlled between 0 to 3 Meters, Do I need to increase the elevation from 0 to 0.3 or 0.5 to control the burst of false positives??
Thanks
Guru