This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: false positives occur at all distances of the radar

Part Number: AWR1843
Other Parts Discussed in Thread: MMWAVE-SDK, DCA1000EVM

Hi

Once every 2.5 seconds to 5 seconds (500 to 1000 frames), there is a problem that false positives occur at all distances of the radar,

and we are investigating.

How to solve it?

Thanks and Best regards,

HaTa.

  • Hello HaTa,

    Could you provide more info? Which application (mmwave SDK demo or TI-Rex lab)? If any of these then default application or with some modification? What is configuration used?

    Regards,

    Jitendra

  • Hi Jitendra

    I put customer's feedback below:

    > Which application (mmwave SDK demo or TI-Rex lab)?

    --> MMWAVE-SDK 3.01.00.02.

    > If any of these then default application or with some modification? What is configuration used?

    --> We modified from MMWAVE-SDK 3.01.00.02. We are using the configuration of two or three advanced frames.

    Thanks and Best regards,

    HaTa.

  • Hello HaTa,

    There can lot more reason for this behaviour. Have they tried default mmw demo (without any change) with new configuration (2/3 advFrame)?

    And on other side they can try same configuration with mmwave studio to capture the RAW ADC data (using DCA1000EVM) and post-process using inbuild Post-proc tool of mmwave studio to verify this discrepancy.

    Regards,

    Jitendra