Hello,
we are experiencing the following issue. (There are a couple of topics in the Forum reporting the same, unfortunately did not help.)
I performed the following installation steps on my Windows 10 laptop:
- mmwave_studio_02_01_01_00
- 32-bit Matlab Runtime Engine 8.5.1
- Microsoft Visual C++ 2013
When done we launched mmWaveStudio (\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime\mmWaveStudio.exe) and this is what we get:
(The first sentence is in italian and means "File format not valid")
Here is the console output:
GM: Constructor
GM: Wed Apr 20 09:34:48 2022
RSTD.Transmit("/Settings")
[09:38:05]
[09:38:05] ### Running Startup script: "C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" ###
[09:38:05] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[09:38:05] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[09:38:05] Scripter ignored: Attempt to UnBuild() again or before Build.
[09:38:05] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[09:38:05] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[09:38:05] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[09:38:05] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[09:38:05] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[09:38:05] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[09:38:05] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\RunTime\\SAL.dll")
[09:38:05] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[09:38:05] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[09:38:05] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[09:38:05] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[09:38:05] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[09:38:05] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[09:38:05] RSTD.Transmit("/")
[09:38:06] RSTD.SaveSettings(): Settings saved to "C:\Users\zinuttir\AppData\Roaming\RSTD\config.xml"
[09:38:06] RSTD.Build()
[09:38:06] RSTD.SaveSettings(): Settings saved to "C:\Users\zinuttir\AppData\Roaming\RSTD\config.xml"
[09:38:06] RSTD.Transmit("/")
[09:38:06] RSTD.AL_Build()
[09:38:06] RSTD.AL_LoadXml()
[09:38:06] RSTD.Transmit("/")
[09:38:06] RSTD.AL_Init()
[09:38:06] RSTD.Clients_Build()
[09:38:06] GM: Init
[09:38:06] GM: Loaded 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\\LabClient.dll'
[09:38:06] GM: 1 Guest (s) init
[09:38:06] GM: 1 Module(s) init
[09:38:06] GM: 2 Tab (s) init
[09:38:06] RSTD.Client_LoadXml()
[09:38:06] [RadarAPI]: ar1.selectRadarMode(0)
[09:38:06] [RadarAPI]: Status: Passed
[09:38:06] Matlab Runtime Engine is installed
[09:38:06] [RadarAPI]: Starting Matlab Engine..
[09:38:13] [RadarAPI]: Matlab Engine Started!
[09:38:14] [RadarAPI]: ar1.selectCascadeMode(0)
[09:38:14] [RadarAPI]: Status: Passed
[09:38:14] [RadarAPI]: ar1.LoadSettings('C:\Users\zinuttir\AppData\Roaming\RSTD\ar1gui.ini')
[09:38:14] [RadarAPI]: Error: Indice oltre i limiti della matrice. *************************
[09:38:14] Trace:
[09:38:14] in AR1xController.ScriptOps.getMatlabPostProcVersion()
[09:38:14] TESTING = false
[09:38:14] RstdNet: Port 2777: Listening..
[09:38:14]
[09:38:14] ***Script completed successfully.***
[09:42:56] RSTD.ShowLogFile()
************************* (Indice oltre i limiti della matrice means "Index beyond matrix limits")
Any idea of what might be causing the issue?
Please notice that we already tried to uninstall and reinstall everything several times and no firewall activity is apparently blocking us.
Thanks,
Riccardo Zinutti