This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Relationship between the XYZ coordinates of radar cloud point and the the XYZ coordinates of a Dielectric Object.

Part Number: AWR1843BOOST

I am trying to use radar to measure the dielectric constant of an object. My understanding is that  the round trip  to the object and back(2D)  is calculated as:

2D= C*T  (C is used as the speed of light in air and T is the Round-trip time) and the calibration is done accordingly.  With the dielectric object, the speed slows based on the dielectric constant, and the Round- trip time changes. My experiments so far indicate that this change in speed is not explicitly accounted for as the distances inside the range bins must remain the same as calibrated. I tried plotting interface angles (air-object) but did not see any effect  My interpretation is that we need the actual round trip time; would you agree?. If this is so, is this available from the raw data? Any help with capturing this data would be very helpful. 

  • Hi,

    Our support team can help you with capturing raw data with the DCA1000 Capture card. However we don't have any experience with your application.

    The TI mmwave sensor works with FMCW modulation. You may want to check academic papers if it is possible to implement your use case with this technology

    thank you

    Cesar

  • Hi  Cesar,

    Thanks for replying and for your patience,  I have checked this out and also have a good understanding of  FMCW Modulation.  We are convinced that your  Technology can do what we are trying once the pertinent data is collected. This may mean some modification to the SW with which I am not very familiar. We have the DCA1000 and would certainly appreciate some help from your Support Team. What is the best way to contact them, would you pass on our conversation and introduce me to one of the Engineers? This would ease the transition.

    This is critical for us and would be a good way to expand the use of your technology.

    Regards

    Lincoln Morant

  • Hi,

    For new topics please start a new thread.

    For DCA1000 information, if there are any issues we have an FAQ:

    [FAQ] DCA1000EVM: DCA1000EVM Debug Resources - Sensors forum - Sensors - TI E2E support forums

    Thank you

    Cesar