This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Capturing data in complex format without DCA1000

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642,

Hello everybody,

I'm starting a work on TI IWR1642 BOOST, For now i'm reading perfectly the data on UART using COM port on the default baud rates (115200 / 921600 ). but this data is on a real format.

In my case i need to gather (capture) the data in the complex format, the aim of that is to build the time-frequency plot from this data so my questions are :

  1. Is there a way to get the complex data on the UART (without using DCA 1000 device)
  2. Can i build the time-frequency spectrogram using the real data (range-doppler Hex data read on UART without DCA 1000)

Please i need an answer ASAP.

Thank you in advance.