This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Max Sample rate of AWR2243

Part Number: AWR2243

Hi expert,

In the ICD document, it mentioned the max sample rate of profile for AWR2243 is 50000 while datesheet said the max sample rate is 45Msps. The driver in SDK also support 50000.

Does it mean we can use 50Msps for 2243?

PF_DIGITAL_OUTPUT_SAMPLING_RATE
2

ADC Sampling rate for this profile is encoded in 2 bytes (16bit unsigned number)
1 LSB = 1 ksps
Valid range:
AWR2243/xWR6243 device: 2000 to 50000 (Max 20MHz IF bandwidth)

Thank you.

Allen