This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: IWR6843ISK-ODS

Part Number: IWR6843ISK-ODS


Hi,

   Tried level sensing example from Toolbox with the visualiser on the web browser. 

The measurement has an error of 100mm, with the range <1m (to the floor & with metal plate on the floor). It (Peak1) is showing 0.884 m against the actual distance of 0.784(approx). Tried default Range depth, width and later changed range depth to  2m & 5m with no change in the measurement value.Looks like this 100mm is an offset, as the difference remains same for change in object's distance from the sensor.

Kindly suggest, where I might need to correct to get exact value(with minimal error) with out offset.

Thanks.