I have the BOOST hooked up to the PC running mmWave demo visualizer. I can see the x-y scatter plot updating as expected.
I am sniffing the AR_MSS_LOGGER pin to get the same data into my micro, It does show the 921600 baud data rate repeating at the frame rate of 10Hz however the packet received does not match the expectations. i.e. the magic header is missing of 0102030405060708 is missing.
Kindly advise if this is the expected starting header for my configuration?