This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Radar not working when changing the transmision anthena Tx on the .cfg file

Part Number: AWR1843BOOST

Hello,

I created a .cfg file using the "Save config to PC" button on the mmwave demo visualizer. This in order to use it again in an external application that simulates the demo visualizer. 

When changing the ChannelCfg between Rx (first parameter) to any array(0x1-15) the configuration still works on the radar and overall it performs well. However changing the second parameter Tx would only work for 0x1 or more(eg 3,5,6,7) but not for independent transmitters e.g 0x2 or 0x4.

Most of the times It would stall after the "Debug: Init Calibration Status = 0x1ffe"  if not I'll get a "Error-1" message

Here is one of the config files that I use. channelCfg 1 7 0, 15 7 0, 2 1 0 work but channelCfg x 2 0 or channelCfg x 4 0 won't.

% ***************************************************************
% Created for SDK ver:03.05
% Created using Visualizer ver:3.5.0.0
% Frequency:77
% Platform:xWR18xx
% Scene Classifier:best_range
% Azimuth Resolution(deg):None (1Rx/1Tx)
% Range Resolution(m):0.244
% Maximum unambiguous Range(m):50
% Maximum Radial Velocity(m/s):1
% Radial velocity resolution(m/s):0.13
% Frame Duration(msec):100
% RF calibration data:None
% Range Detection Threshold (dB):15
% Doppler Detection Threshold (dB):15
% Range Peak Grouping:enabled
% Doppler Peak Grouping:enabled
% Static clutter removal:disabled
% Angle of Arrival FoV: Full FoV
% Range FoV: Full FoV
% Doppler FoV: Full FoV
% ***************************************************************
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 1 1 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 77 945 7 28.49 0 0 30 1 256 12499 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 0
frameCfg 0 0 16 0 100 1 0
lowPower 0 0
guiMonitor -1 0 1 0 0 0 0
cfarCfg -1 0 2 8 4 3 0 15 1
cfarCfg -1 1 0 4 2 3 1 15 1
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
lvdsStreamCfg -1 0 0 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 4 63 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 49.99
cfarFovCfg -1 1 -1 1.00
calibData 0 0 0
sensorStart