Part Number: OPT3001-Q1
Hi Expert
My customer have two question about full-scales:
1. I know this device Measurements is 0.01 Lux to 83k Lux, if environment like direct sun more than 83K whether damage device?
2. in the HUD application, when the driving direction of the car is opposite to the direction of the sun, device will get lower Lux but environment light very high because diffuse earth.
so do we have any method to calibrate this error?