TMP 117 unique NIST # for example is Presented as Serial Number 0xD6510F8416F1 EEPROM1 contains 0xD651 EEPROM2 contains 0x0F84 EEPROM3 contains 0x16F1 Presented as Serial Number 0xD6510F8416F1 The answer confirms that these are the correct three bytes to include for the complete Serial Number (Unique ID), but it does not confirm that this is the correct Serial Number representation (byte order, endian-ness etc)? If you could provide a reference description for the Serial Number format that would be great, but confirmation of this example's correctness would also be very useful