Other Parts Discussed in Thread: FDC1004
I am working on a design where I believe I would like to use a Mutual Capacitance matrix (maybe 8x8). The dielectric between our X (horizontal) and Y (Vertical) grids is compressible and I would like to measure the increase in capacitance as areas of the grid become compressed while being isolated from any external signals. I ordered the FDC1004EVM just to get some values to prove the concept. I do not think this is the best device for my needs and it also does not have enough channels. I have read through your design guide at https://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/CapTIvate_Design_Center/1_83_00_08/exports/docs/users_guide/html/CapTIvate_Technology_Guide_html/markdown/ch_basics.html and found it to be very helpful.
I should not need to measure above 16pF though the ability to have an offset is helpful. I need to detect multiple points of contact. I would like at least an 8x8 Matrix. Picking up signals from any distance is actually a hinderance so an isolated signal with higher resolution would be great.
Any help selecting the best device for this application would be greatly appreciated.