Other Parts Discussed in Thread: AWR1642BOOST-ODS
Hi,
While testing for target configuration, i tested to check connection, which displayed as follows :
The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.
The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.
[End: Texas Instruments XDS110 USB Debug Probe_0]
I explicityly installed XDS110 as well but still then in device manager i dont see the COM port of XDS110 as shown below :

How do i get this XDS110 recognized for AWR6843AOP. Additinally how do i download mmwave demo built , using CCS 11.2?
Regards
Vinay