In automotive lab demo mrr, the default setting of VCO is VCO1, therefore the frequency range should be 76~78GHz (bandwidth: 2GHz).
However, in the parameters settings of USRR mode: USRR20 and USRR30, it seems the bandwidth set for the ramp of chirp signal is larger than 2GHz.
Can you please check if this is correct?
MODE | DETECTION DISTANCE | START_FREQ_GHZ | RAMP_END_TIME_VAL(us) | FREQ_SLOPE_MHZ_PER_US(mhz/us) | bandwidth(mhz) |
MRR | 80 | 76.01 | 56 | 8 | 448 |
120 | 76.01 | 60 | 4 | 240 | |
USRR | 20 | 77.01 | 87.28 | 42 | 3665.76 |
30 | 77.01 | 44 | 56.25 | 2475 | |
50 | 77.01 | 44 | 37.5 | 1650 |