Other Parts Discussed in Thread: AWR1843
I have two questions below.
(1) Assume that an object in a Range is detected using AWR1843.
At this time, the width of the object in the x-axis direction and the width in the z-axis direction are respectively
Is it okay to think that it can be obtained by 2*R*Wx and 2*R*Wz?
(Wx: Angle of Azimuth, Wz: Angle of Elevation)
If it is different, I would be happy if you could also tell me the derivation process.
(2) When detecting the width of an object with AWR1843
If you want to find the width of each x-z axis direction seen from Radar using AWR1843,
Do you need to look at the difference in the x-axis and z-axis of the object in multiple frames?