This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5032: the power consumption in 3V

Part Number: DRV5032

Hi team,

What is the power consumption in 5Hz with 3V supply?
My customer cares a lot about the power consumption and i only found the consumption at 5Hz with 1.8V. 

Or do u have better advice of hall sensors with lower power consumption?

  • Zoey,

    Thank you for reaching out on E2E.  The 5Hz version of DRV5032 is in the FB package:

    Looking at the electrical specification table for the DRV5032 FB sensor, we find the average consumption at 1.8, 3, and 5V.

    Thanks,

    Scott