This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2022: How to estimate the error of HDC2022 for 1 year?

Part Number: HDC2022


Hi,

can anyone answer below questions?

Q1) I am going to use HDC2022 in 80% RH @ 10C, and trying to estimate the error for one year as below, please confirm? my application requires the error should be less than 5% RH.

HDC2022 worst case error = 2%(accuracy for <80% RH) + 1%(hysteresis) + 0.25% (drift for 1 year) =3.25% RH

Q2) I read the long term drift of HDC2022 is 0.25% RH positive side ( +0.25 %RH /year) from one of the post, is that true? 

Q3) The datasheet has typical spec i.e. LTD, Hysteresis, accuracy etc., what are the approximate maximum numbers?

Q4) Is there any way to measure the LTD for my application (test fixture) by stressing the sensor thermally?