This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: COM ports not showing up as XDS110 Class as shown in the user guide

Part Number: MMWCAS-DSP-EVM

Hi,

I am trying to connect to the device using the mmWave Studio. I have installed the drivers provided in the ftdi directory, however the two virtual ports appear differently (shown below) to the example provided in the mmWave Studio user guide. I am not sure if my hardware should appear as XDS, but it the mmWave Studio GUI, the `No. of devices connected' remains 0. I am able to connect via CLI (PuTTy). I have removed all older virtual COM ports and followed the information provided in (+) MMWCAS-DSP-EVM: Problems with communicating to the board via ethernet and serial port - Sensors forum - Sensors - TI E2E support forums. Please assist.