This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: IWR6843ISK

Part Number: IWR6843ISK

Hi, 

I'd like to use baud rates higher than 921600 in mmwave demo visualizer 3.6.0 for TI IWR6843ISK.  I tried baud rates of either 1843200 or 3125000 that are the recommended rates other than 921600 as per mmwave SDK user guide 

Since these rates are not available in the drop-down provided in Visualizer, I used the custom option available to specify the baud rate. However, I am getting an error as shown below. I can connect using any other baud rate options provided in the drop-down. Just baud rates higher than 921600 have this problem

Can you help me to solve this?