This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01012: Syncronising external camera to radar frames

Part Number: TIDEP-01012


Hello TI Team,

I am trying to synchronize an external camera with the mmWave Cascade radar. Ideally, each frame of the camera should coincide with a frame from the radar. There are already posts on this topic see:

https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1043977/tidep-01012-help-for-external-triggering-on-cascade-radar

https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/878236/tidep-01012-cascade-imaging-radar-sync-log-with-camera

But these appear to relate to triggering the radar from an external source, for my application I need the radar to act as a trigger to the external source. According to the documentation there is a GPIO7_27 pin labelled AWR Extern SYNC, would this pin output a signal at the start of each frame? Additionally, if this pin could be used as a trigger for an external device, where is the pin physically located, as it is not labelled in any diagrams?

 

I look forward to your response.

Sincerely.

DS