Other Parts Discussed in Thread: IWRL6432
Hi,
I am using the IWRL6432 sensor board, and I have the following queries:
- Is it possible to generate configuration files using mmWave Low Power Visualizer 5.2 (mmWave Radar Visualizer 5.2.0)?
- I am looking for a method to generate these files.
- How can I access the source code of the low power visualizer (mmWave Radar Visualizer 5.2.0)?
- I require it to locate the equations used for calculating range profiler, range doppler, and other parameters.
- Does the app use a single port(config port), or does it use both data and config port?
- In the app, it only asks to specify the config port.
Regards
Aditya