This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Question regarding the sending of Config to mmWave Device

Part Number: IWR6843AOPEVM

Hi,

I'm using the IWR6843AOPEVM sensor with the flashed the AOP binary located at <RADAR_TOOLBOX>\source\ti\examples\Out_Of_Box_Demo\prebuilt_binaries\out_of_box_6843_aop.bin. 

I'm new to using these sensors and want to configure them to the "Best Velocity Resolution" present in the mmWave Demo Visualizer. However, when I send config to mmWave device the console shows that all the configurations are skipped.  Full console output shown at the bottom of this post. 

  

I know something is happening since I'm able to view the plots, and they respond to motion in front of the sensor. My question is are the configurations that I have set within the visualizer being loaded? 

Full console output:

mmwDemo:/>% ***************************************************************
Skipped

mmwDemo:/>% Created for SDK ver:03.06
Skipped

mmwDemo:/>% Created using Visualizer ver:3.6.0.0
Skipped

mmwDemo:/>% Frequency:60
Skipped

mmwDemo:/>% Platform:xWR68xx_AOP
Skipped

mmwDemo:/>% Scene Classifier:best_vel_res
Skipped

mmwDemo:/>% Azimuth Resolution(deg):30 + 30
Skipped

mmwDemo:/>% Range Resolution(m):0.214
Skipped

mmwDemo:/>% Maximum unambiguous Range(m):10.95
Skipped

mmwDemo:/>% Maximum Radial Velocity(m/s):3.84
Skipped

mmwDemo:/>% Radial velocity resolution(m/s):0.06
Skipped

mmwDemo:/>% Frame Duration(msec):100
Skipped

mmwDemo:/>% RF calibration data:None
Skipped

mmwDemo:/>% Range Detection Threshold (dB):15
Skipped

mmwDemo:/>% Doppler Detection Threshold (dB):15
Skipped

mmwDemo:/>% Range Peak Grouping:enabled
Skipped

mmwDemo:/>% Doppler Peak Grouping:enabled
Skipped

mmwDemo:/>% Static clutter removal:disabled
Skipped

mmwDemo:/>% Angle of Arrival FoV: Full FoV
Skipped

mmwDemo:/>% Range FoV: Full FoV
Skipped

mmwDemo:/>% Doppler FoV: Full FoV
Skipped

mmwDemo:/>% ***************************************************************
Skipped

mmwDemo:/>sensorStop
Ignored: Sensor is already stopped

Done

mmwDemo:/>flushCfg
Done

mmwDemo:/>dfeDataOutputMode 1
Done

mmwDemo:/>channelCfg 15 7 0
Done

mmwDemo:/>adcCfg 2 1
Done

mmwDemo:/>adcbufCfg -1 0 1 1 1
Done

mmwDemo:/>profileCfg 0 60 115 7 15 0 0 100 1 64 9142 0 0 158
Done

mmwDemo:/>chirpCfg 0 0 0 0 0 0 0 1
Done

mmwDemo:/>chirpCfg 1 1 0 0 0 0 0 2
Done

mmwDemo:/>chirpCfg 2 2 0 0 0 0 0 4
Done

mmwDemo:/>frameCfg 0 2 128 0 100 1 0
Done

mmwDemo:/>lowPower 0 0
Done

mmwDemo:/>guiMonitor -1 1 1 0 0 0 1
Done

mmwDemo:/>cfarCfg -1 0 2 8 4 3 0 15 1
Done

mmwDemo:/>cfarCfg -1 1 0 8 4 4 1 15 1
Done

mmwDemo:/>multiObjBeamForming -1 1 0.5
Done

mmwDemo:/>clutterRemoval -1 0
Done

mmwDemo:/>calibDcRangeSig -1 0 -5 8 256
Done

mmwDemo:/>extendedMaxVelocity -1 0
Done

mmwDemo:/>lvdsStreamCfg -1 0 0 0
Done

mmwDemo:/>compRangeBiasAndRxChanPhase 0.0 1 0 -1 0 1 0 -1 0 1 0 -1 0 1 0 -1 0 1 0 -1 0 1 0 -1 0
Done

mmwDemo:/>measureRangeBiasAndRxChanPhase 0 1.5 0.2
Done

mmwDemo:/>CQRxSatMonitor 0 3 4 19 0
Done

mmwDemo:/>CQSigImgMonitor 0 31 4
Done

mmwDemo:/>analogMonitor 0 0
Done

mmwDemo:/>aoaFovCfg -1 -90 90 -90 90
Done

mmwDemo:/>cfarFovCfg -1 0 0 10.97
Done

mmwDemo:/>cfarFovCfg -1 1 -3.2 3.20
Done

mmwDemo:/>calibData 0 0 0
Done

mmwDemo:/>sensorStart
Debug: Init Calibration Status = 0x1ffe

Done