This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
HW: AWR2944 ES2.0 EVM, DCA1000 EVM
SW: AWR2944 HECR package based on SDK 4.4, Studio CLI, mmWave Studio 3.1
Could you provide a document to describe how to capture ADC raw data when using AWR2944 HECR demo?
I didn't find proper documents in Studio CLI/mmWave SDK 4.4/mmWave Studio 3.1
In the Studio CLI, the document only mention those AWR1xxx but no AWR2944.
In mmWave SDK 4.4, it only points to Studio CLI.
In the mmWave Stuido 3.1, it doesn't mention AWR2944 too much, could we use mmWave Studio + DCA1000 like before? or we have to use Studio CLI + DCA1000?
In related E2E discussion thread, it looks using mmWave Studio GUI + DCA1000 to do AWR2944 ADC raw data capture is no longer supported, no pretty sure if it's still valid today?
Base on above observation, I do need to a document to describe how to get ADC raw data when using HECR package based on SDK4.4.
Thank you.
Hi James,
We have published mmWave Studio to support AWR294x device.
https://www.ti.com/tool/download/MMWAVE-STUDIO-2G (03.01.01.00)
Customer can use this tool with DCA1000EVM to configure then capture raw ADC data.
Regards,
Jitendra
Hi Jiten,
Actually, I've tried https://www.ti.com/tool/download/MMWAVE-STUDIO-2G (03.01.01.00) few days ago but I can't connect RS232 COM port.
The error message is like:
The setup is like:
Except XDS-USB port, I also tried to plug USB to FTDI-USB on AWR2944EVM and use those COM port but none of them is working.
That's really strange because I can use AWR1642/AWR1843/AWRL1432/AWRL6432 to do the DCA1000 capture but the same procedure doesn't work on AWR2944...
Finally, I made it work. The root cause is that you can't connect FTDI-USB port in advance. You need to wait DCA1000 and AWR2944 EVM reset ready and then plug in usb cable to FTDI-USB port. If you connect everything in advance, it won't work.