This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: IWR1642 interfacing the device using MATLAB GUI

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642

Hi team,

1. I am working on people count project using IWR1642. I was able to run the demo image and visualize the output using Matlab GUI. But when I execute the same on the Matlab code, it throws an error message "error while evaluating uicontrol call back".
2. I would like to read the output data using a serial monitor from IWR 1642. How can I do this?
3. How can I interface Lauchpad with IWR 1642 and read the output data? Is there any demo?

Could you help?

Thanks & Regards,

Vivian