Other Parts Discussed in Thread: MMWAVEICBOOST
Hi Expert,
I am posting this in behalf of the customer.
I have IWR6843AOPEVM, and I want the CLI command set while the main program is built. i.e. when power on IWR6843AOPEVM hardware, start detection and does not require to external CLI command
Is there any example available for this?
I want an example for this IWR6843AOPEVM device. But I don't want to send external CLI command. I want to send a command in the main build
for example when I upload the 3d_people_count.bin file in this hardware:- in this bin file already set CLI command
And not required to give external cli command on UART port.
And I am writing on this Uart command Handler:- gMmwMssMCB.commandUartHandle
[It writes on command UART but the sensor is not starting and not getting any response
I am using XDS of mmWaveICBOOST AND port 13, baud rate 115200

Best regards,
Jonathan