This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Increasing distance

Part Number: IWR6843ISK


Hello!

We took the recommendations from the previous thread and got improvements.

We have additional questions:

  1. Does TI have a traffic monitoring firmware that emits three TX channels to achieve maximum range?
  2. Is there technical documentation for firmware 68xx_traffic_monitoring_70m_MIMO_2D?
  3. In our experiments, we use firmware BSS - xwr68xx_radarss.bin and MSS - xwr68xx_masterss.bin, with standard default settings, we get an unambiguous speed measurement in a small range of +-7 m/s. Does TI have firmware for measuring speeds +-50 m/s?
  4. To increase the range of the radar, TI recommended that we use an antenna lens, or similar device. Does TI have reference drawings for this device. Or the part number of the device available for purchase?
  5. If we manage to increase the range of the radar, with what firmware and settings will we be able to see the original signals and process them in TMC?

Thank you.