Hello everyone,
I am trying to design a 3-phase EV charger circuit so i need to add a ground detection and leakage detection to my design.
I searhed through net and found AFE3010 ic, and looked into its referance schematic in datasheet. And referance to that, i would like to change some components etc. in order to make it compatible with 3 phase 400VAC system(if it is possible of course).
And if it is not possible to implement a 3ph system with this ic, it would be awesome if you point out different ICs or different designs.
Also attached an excel sheet for 220VAC tweak guide for referance schematic that had been shared by Peter Iliya at below thread.
AFE3010-BOM_5F00_calculations.xlsx
I am in need of some assistance about this adventure of mine :)
Thanks in advance.