This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: DCA1000 not working

Part Number: DCA1000EVM
Other Parts Discussed in Thread: AWR1843BOOST, AWR1843

Dear members,

I was working on calibrating the radar for AWR1843 chip. But when i connect AWR1843Boost EVM to DCA1000. Its not reading the DCA1000's firmware version. Always the command timeout occurs.

All the LEDs on DCA1000 are always on. So i suppose firmware could be the issue.

I got the diamond programmer and tried reflashing the board. as per the steps provided in the user manual.

The Flash erase command ran successfully.

but when programming the Flash chip. It responses with

"ERROR - Programming failed.

IDCode Checking...

ERROR - Verification Error...when Processing function: 'CHECK_ID'

ERROR - Operation: unsuccessful.

"

OR

"INFO - Check configuration setup: Start.

Device#1 LFE5UM-85F: Shift out '1' instead of '0' from Bypass register.

ERROR - Check configuration setup: Unsuccessful.

ERROR - Programming failed.

"

One of these 2 errors i am getting.

Please help me out in resolving the issue and get it working.

Or is there any other way i can calibrate the radar for AWR1843. without using DCA1000.

Regards

Kunal