Other Parts Discussed in Thread: MMWCAS-RF-EVM
Hi,
I noticed that there are four lua scripts for MMWCAS-RF-EVM configuration, which are "Cascade_Configuration_Basic.lua", "Cascade_Configuration_MIMO.lua", "Cascade_Configuration_TestSource.lua", "Cascade_Configuration_TXBF.lua".
I only know "Cascade_Configuration_TXBF.lua" and "Cascade_Configuration_MIMO.lua" are corresponding to the TX beamforming mode and MIMO mode of MMWCAS-RF-EVM,
but I want to ask:
1. What are "Cascade_Configuration_Basic.lua" and "Cascade_Configuration_TestSource.lua" used for?
2. If I disable the test source in "Cascade_Configuration_TestSource.lua", can I use it to configure the radar? If yes, will the radar be configured to MIMO mode or TXBF mode?
3. If I want to detect object around 3 meters away from the sensor, which lua script should I use? Using the default chirp parameters in "Cascade_Configuration_MIMO.lua", the max range I calculated is 13.66m and range resolution is 0.0474m, can you please help me to confirm?
Regards,
Chennan