Part Number: IWRL6432
Other Parts Discussed in Thread: INA228, ,
The IWRL6432BOOST Evaluation Module can measure the power consumed by the IWRL6432 device in operation through the 4 current measurement amplifiers (INA228's) placed on the board. However, the measurement is ONLY valid for certain board revisions. Currently, there are 3 board revisions that have been produced
Rev A
Rev B
Rev B, ASSY A1
| Revision | Pictures | Can it measure power accurately? |
|
Rev A |
![]() |
NO |
| Rev B | ![]() |
NO |
| Rev B, ASSY A1 | ![]() |
YES |
EVMs that CANNOT measure power accurately can be modified to measure power accurately through the following BOM changes outlined in section 5 of the xWRL6432 Power Consumption App Note