Other Parts Discussed in Thread: IWR6843AOP
Hi
We are trying to configure and test IWR6843AOP and see the board's performance in the 3D people counting demo.
The board configuration is selected from \ti\mmwave_industrial_toolbox_4_12_1\labs\People_Counting\3D_People_Counting\chirp_configs\AOP_6m_default
The prebuilt binary files are selected from:
C:\ti\mmwave_industrial_toolbox_4_12_1\labs\People_Counting\3D_People_Counting\prebuilt_binaries\3D_people_count_68xx_demo
The visualizer is from radar_toolbox_1_20_00_11\tools\visualizers\Industrial_Visualizer\mmWave_Industrial Visualize.exe
(please note the visualizer is selected from radar_toolbox_1_20_00_11 and not mmwave_industrial_toolbox_4_12_1)
When the device is connected, an error or warning raises:
"Warning: Frame packet length read is not equal to totalPacketLen in frame header. Subsequent frames may be dropped.
Parsing Error on frame: 187
Error Number: 3"
or sometimes this error is raised:
"Frame packet length read is not equal to totalPacketLen in frame header. Subsequent frames may be dropped.
Parsing Error on frame: 95"
Any thoughts on the cause(s) of this error or warning?