As shown in the figure, spi is multiplexed as normal gpio and set to output mode using the GPIO_setConfig function. However, high and low levels cannot be written using GPIO_write.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As shown in the figure, spi is multiplexed as normal gpio and set to output mode using the GPIO_setConfig function. However, high and low levels cannot be written using GPIO_write.
Hello,
I will be responding to the question in the second thread made on this topic due to it being the same subject while also stating a question.
Best Regards,
Pedrhom