This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6243: Flashing guide specific to IWR6243

Part Number: IWR6243
Other Parts Discussed in Thread: AWR2243, UNIFLASH, AWR1243

We are currently testing a custom board with IWR6243.

For flashing the IWR6243, our main source of information is "AWR2243 bootloader flow". Currently our method of flashing is the following:

  • use UniFlash (latest), select AWR1243 from the device list (because of this thread, in order to flash a single meta-image)
  • use xwr62xx_metaImage.bin from IWR6243 DFP (following AWR2243 bootloader flow section 3.1: "In ES3.0, the two images are combined into a single meta-image")
  • flash the single meta-image.

Is this the correct method to flash the IWR6243 in a testing / production environment ?

How can we check after reboot that it was correctly programmed and boots as it should ? (apart from initiating the control interface via SPI)