This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Configurable CSI Pins

Part Number: AWR2243
Other Parts Discussed in Thread: AWR2944,

Hello,

do I understand it correctly from the data sheet, that the CSI data lanes and clock lane can be configuered to different Pins via internal multiplexing (to adapt the signals for a better layout routing)?

If yes, can you please let me know in which register this can be conficured? 

Thank you.

  • Dear Max - 

    Thanks for the post and welcome to E2E!

    The AWR2243 is not re-configurable with regards to the pins - meaning, there is no pinmux for this device, which is why there is no pinmux table, like you might have seen for the AWR2944 device, but even on that device, the CSI2 and LVDS lines have dedicated pins