Part Number: IWR6843AOPEVM
Other Parts Discussed in Thread: MMWAVE-SDK
Good afternoon,
I am currently working with the IWR6843AOPEVM. I have followed the procedure outlined in this link: https://dev.ti.com/tirex/content/radar_toolbox_1_30_01_03/source/ti/examples/Robotics/ros_driver/docs/TI_mmWave_ROS_Driver_Users_Guide.html to visualize point cloud information using ROS.
While the point clouds are being published, I am encountering the following two issues:
1. The point clouds are only published when the obstacle or the board is in movement. I would assume this is an defined behaviour and based on the configuration files, but we would like to detect the static surrounding as well and I cannot follow/understand the configuration parameters completely.
2. The parameters are not initialized when I run the ros1driver package using the command: roslaunch ti_mmwave_rospkg 6843_multi_3d_0.launch.

We loaded the default configuration files of 6843_multi_3d.cfg and similiar configs.
We also looked in the issue https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1223354/iwr6843aopevm-lab-resource-example-issue, but this also did not solve the configuration. The values changed with the different position of the incrementation, but most values were inf or 0 most of the times.
I would appreciate any assistance or guidance you can provide to resolve these issues.
Thank you for your help.
Best regards,