Other Parts Discussed in Thread: IWR6843ISK, , MMWAVEICBOOST, IWR6843
I am working to set up DCA1000EVM to extract real time data from IWR6843ISK board with mmwaveICBoost. I followed the user guide, set all the switches to correct value, connected all the cables. However, after powered on, I can see the two XDS ports correctly in device manager, but couldn't see the four ftdi ports as indicted in the users guide:
What I got was:
Correct XDS ports, but missing all four ftdi ports:

however, there is an unknown USB device list there:

this devices should be related to the DCA1000EVM ftdi ports because when I unplug the micro USB cable connected between DCA1000EVM and laptop, it is gone; when I plug in the micro USB cable to laptop, laptop shows a message saying can't recognize the USB device.
I tried to update driver software using the ftdi directory under MMWAVE_Studio installation directory, it didn't solve problem, still device not recognized.
Below are my setup, please help me to find out what's wrong. Thanks!

Because in the above image, two boards are overlapped, I also have a pic with two boards seperated.







I couldn't find all these files and paths at all. Do I need to install any other files on my PC? Also, I am using