Part Number: DCA1000EVM
Hello,
I am working with the AWR2243BOOST board and DCA1000EVM, for real-time data processing. It was mentioned in the mmWave software user guide that after 1 GB of captured data the DCA1000 will start capturing the data to a new file.
So I was wondering where to find in the source code the configuration referred to the size of the captured file after which the DCA1000 starts capturing the data to a new file??
Also, is it possible to modify this amount from 1 GB to the amount needed to capture 1 frame only or a certain set of frames in which I can already start processing the captured frames while the DCA1000 is collecting and appending the new files of the captured data?
Best regards