Other Parts Discussed in Thread: LM95213,
Hi,
Our customer is considering changing from LM95213 to LM95233.
Therefore, I have the following inquiry, so please let me know.
- A register called Diode model select (0x30) has been added to LM95233.
1) Is there any need to change the software?
2) If the default value of the register after POR is 0x20 and nothing is set (just replaced from LM95213), Remote 1 is
“TruTherm BJT beta compensation technology enabled” setting
Also, is it correct to understand that Remote 2 is disabled?
3) If Remote 2 is enabled and MMBT3904 is connected, what will happen to the measurement accuracy?
In the Applications Hints of the data sheet, MMBT3904 is also included when enabled.
There was a statement that it would be optimized, so I'm curious as to what will happen.
4) Connect a processor other than MMBT3904 or Intel to Remote when disabled
Am I correct in understanding that the measurement accuracy when doing this is the same as the LM95213?
Best regards,
Hiroshi
Hiroshi