This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWRL1432BOOST: There are some errors when debug awrl1432. We can not halt into mmwave_demo task.

Part Number: AWRL1432BOOST
Other Parts Discussed in Thread: IWRL6432, AWRL1432

Cortex_M4_0: Can't Run Target CPU: (Error -1268 @ 0x1090001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 12.6.0.00029)

We need to check whether all the switches are correct.

We are using the built-in project and have not made any modifications.

And We have encountered the same issue in forum about iwrl6432.

IWRL6432BOOST: IWRL6432BOOST ccs Cortex_M4_0: Can't Run Target CPU: (Error -1268 @ 0x1090001) Device is locked up in Hard Fault or in NMI. - Sensors forum - Sensors - TI E2E support forums

Can I seek some assistance?

BR,

Wayne