This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: XWR1X43BOOST board, DCA1000EVM, two 5V power adapters, 2 USB to micro-USB cables, 1 ethernet cable, 1 USB C to Gigabit Ethernet adapter

Part Number: DCA1000EVM


Hi E2E,

I just downloaded mmWave 2.1.1.0 and I have this error when opening it. I made sure to download MATLAB runtime R2015aSP1 (8.5.1) and the XDS Emulation Software. 

...

[03:53:35] Matlab Runtime Engine is installed
[03:53:35] [RadarAPI]: Starting Matlab Engine..
[03:53:40] [RadarAPI]: Matlab Engine Started!
[03:53:43] [RadarAPI]: ar1.selectCascadeMode(0)
[03:53:43] [RadarAPI]: Status: Passed
[03:53:43] [RadarAPI]: ar1.LoadSettings('C:\Users\ubci\AppData\Roaming\RSTD\ar1gui.ini')
[03:53:43] [RadarAPI]: Error: L'index se trouve en dehors des limites du tableau.
[03:53:43] Trace:
[03:53:43] à AR1xController.ScriptOps.getMatlabPostProcVersion()
[03:53:43] TESTING = false
[03:53:43] RstdNet: Port 2777: Listening..
[03:53:43]
[03:53:43] ***Script completed successfully.***

Any help will be greatly appreciated. Thanks a lot.