Other Parts Discussed in Thread: AWRL6432AOP
Hello
We recently received five samples of the IWRL6432AOP. And five test boards were produced.
However, only two of the five units operate normally (image flashing and radar operation), and the remaining three units do not operate (image flashing does not work either). Here's what we checked:
1. Check UART communication: no problem
2. Since two units operate, there is no problem with the circuit configuration.
Next, here's what we did:
1. After flashing the image, I removed the flash memory from the board that was operating normally and assembled the removed memory onto the board that was not working.
2. And check that it is operating normally: It does not start from booting.
So we determined that the default boot loader was not included in the chip we received as a sample.
If you have any experience resolving situations like this, I would appreciate your suggestions on how to resolve them.
If the chip is the problem, I wonder if we can provide additional sample chips (AWRL6432AOP or IWRL6432AOP) from TI.