Other Parts Discussed in Thread: AWR1642,
How the maximum detection distance by AWRL 1432 which support on Entry-BSD application of own design antenna?
1. We would like to study AWRL 1432 for entry BSD function, need to evaluate the maximum detection distance, how it is if we use our own design antenna from EVK 2 patch to 6 patch (~3dB improve)?
2. MCU is Cortex-M4F at 160MHz instead of Cortex-R4F at 200MHz if we compare with AWR1642, what limitation need to consider? e.g. The data output rate 40Hz to 20Hz (DSS handle object) ...etc?
3. AWRL1432 remove DSP but add HWA for FFT, CFAR..etc if we compare with AWR1642 with DSP, what limitation need to consider?
Many thanks on this evaluation.